Part Number: ADS8688A
Other Parts Discussed in Thread: ADS8568, ADS114S08B, ADS8686S, ADS114S08
I'm currently working on a data acquisition system and the ADS8688A looks like an incredible device.
I'm currently trying to sample:
- Load Cell (10V excitation)
- Pressure Transducers (0-5V)
- Thermocouples (+- 6 mV)
The ADS8688A's multiple range selection is incredible, and the analog front end's low pass filter helps with skimping out on some RC filters, but the problem is that the GND inputs all must be within 0.1V of each other. This makes it difficult to use the load cell, where the output is differential between its leads, but the leads individually to ground may be up to the excitation voltage of 10V.
Is there a chip that that has all the multiple ranges and analog front end of ADS8688A but is differential (so that the negative ends don't all need to be equal-ish to GND and each other)? If not I think this chip will be really useful for DAQ systems where a whole lot of voltage ranges are needed, but the number of each is not known at design time.