Other Parts Discussed in Thread: DAC5662
Hello,
I will use DAC5662EVM to check behavior of DAC and transformer circuit.
I want to check if the output voltage swing from the J1 connector on DAC5662EVM is 0.5Vpp within the transformer band (P/N:T1-1T-KK81 0.08 to 200MHz).
Input data to DAC5662 is below and circuit of DAC5662EVM is not changed.
<DAC input>
sin wave data 0x000 to 0xFFF
sine wave frequency 100kHz to 150MHz
Regards,
MESH