In a previous thread, I asked for some details regarding the Absolute Input Current vs Differential Input Current. I received a very detailed reply, but there are some follow-up points I'd like to confirm for the customer.
Taking Figure 10 and 14 as examples from the Datasheet, you can see that the current can be both "positive" and "negative". Is my understanding correct?↓
- When a pin's absolute input current is positive, it is "sinking" current into the pin - in this case, it draws some current away from the IDAC source, causing small errors. (voltage drop across AINx pin's series resistor means the voltage at AINx is slightly lower than the other side of the resistor)
- When a pin's absolute input current is negative, it is "sourcing" current out of the pin - in this case, it adds more current into the IDAC path (voltage drop across AINx pin's series resistor means the voltage at AINx is slightly higher than the other side of the resistor)
- The differential input current can be + or -, but it is the absolute input current that dictates if a pin is sinking/sourcing current - yes?
Thanks,
Darren