Other Parts Discussed in Thread: ISO7740, ISO7840
Hello Team,
My customer is looking for the best-fit SPI digital Isolator for ADS127L01. Can you suggest one?
Regards,
Renan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Renan,
The typical clock speed for CLK and SCLK is 16.384MHz, which results in a clock period of 61nS. In order to minimize the number of isolator channels, a prop delay less than 30nS, and pulse distortion less than 5nS should be used. There are several TI isolators that can meet this requirement.
ISO7740, ISO7640, and ISO7840 families of isolators should all work for SPI isolation. If using a slower main clock, then the timing requirements are further relaxed and lower prop delay devices can be used.
Regards,
Keith Nicholas
Precision ADC Applications