This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 1
Views: 97
Part Number: TPL1401
How can I use the TPL1401 to add a programmable gain to my signal?
Best,
Katlynne Jones
The TPL1401 can be used for programable gain. For this application, use VDD as the reference for the device, and apply the input signal to VDD. VDD is used as the reference by default, so there are no configuration settings that need to be modified. Because the signal is being applied to the VDD input, the signal will need to be in the valid 1.8V to 5.5V supply range of the TPL1401. A common use for this circuit is to tune audio circuits such as microphone sensitivity.
With VDD = VIN, the output signal will have an attenuation of 1 to 1/256 based on the TPL1401 transfer function of:
DPOT_POS will range from 1 to 256 to select the gain. Write the desired code to the DPOT_POS bits in the DPOT_POSITION register. The gain setting can be saved in the nonvolatile memory of the TPL1401 to allow for operation without a processor after initial programming. To save the value in the NVM view: [FAQ] How to generate a DC setpoint or bias using the TPL1401?
(Register table taken from TPL1401 datasheet version * Sept 2020)
The TPL1401 can be found in many common applications:
End equipment
Url
Exit and emergency lighting
www.ti.com/.../exit-emergency-lighting
Barcode scanners
www.ti.com/.../barcode-scanner
Barcode readers
www.ti.com/.../barcode-reader
Smart speakers
www.ti.com/.../smart-speaker
Video doorbells
www.ti.com/.../video-doorbell
Cordless vacuum cleaners
www.ti.com/.../cordless-vacuum-cleaner
Robotic lawn mowers
www.ti.com/.../robotic-lawn-mower
Laser distance meter
www.ti.com/.../laser-distance-meter
You can find some additional information about the TPL1401 here:
TPL1401
TPL1401EVM
You can find more information about precision DACs here:
Precision DAC Learning Center
www.ti.com/.../learning-center.html
TI Precision Labs - DACs
training.ti.com/ti-precision-labs-dacs
Data Converter Circuit Cookbook
www.ti.com/.../data-converter-circuits.html