Hi all! Can someone please help? I am using the ADS1263 EVM daughter card.
I can write and read back successfully from the registers. But when I read the ADC value, all 6 bytes were 0 including the STATUS and CHECKSUM !
I chose the pulse conversion mode. The START signal is every 2 ms. (channel 1)
The DRDY goes low after 1.2 ms after started. (channel 2)
Then I read the 6 data bytes at once, but all 0. (channel 3 is the SCK, and 4 is the DOUT)
I got it work before. One day it failed as described above. So I replaced the ADS1263. Remained the same. May be I made some mistakes in the software accidentally, but the register values are the same. Seems not software problem.
I just found I could not read back the registers when the CLOCK SELECT SWITCH was on the XTAL side. And I probed at pin 15 and the crystal pin, no oscillation found.
Then I switched to use INTERNAL oscillator, it worked as described above. Will it be the cause? Or it is another problem?
Thank you for helping me to solve these problems. Thank you!