Other Parts Discussed in Thread: TMS320F28374S, AMC1200, AMC1303E2520, AMC1303E2510
Hi,
I'm starting a new project and I'm switching form Microchip to TI C2000 Delfino class probably to the - TMS320F28374S. I already used AMC1200 isolation op amp for current measurement and I had good results. Now I'm thinking of going with AMC1306E25 & the DSPs SDFM and I have a couple of questions about the use of a delta sigma adc.
1) I have seen that there is a Manchester coded option for the DOUT. With this I don't have to run a CLK line form the DSP to the ADC - this is a positive. Are there any negatives in using a Manchester option?
2) The datasheet says 16 bits of resolution at a data rate of 78 kSPS. Is this the recommended speed/resolution of operation? As I understand, if i set the filters in the DSP differently I can get lower resolution but faster sample rate right?
3) In the data sheet the clock is listed to be between 5 and 20 Mhz. What would be the TYP clk? The DSPs SDFM works to 25 MHz. Is there any reason why would I not run the ADC at 20 MHz (besides power consumption and EMC)?
4) If I use the Manchester coded setting, and want to use multiple ADC, can I use multiple different clocks or do the clock have to be synchronised (more of a TMS320F28374S question)?
Best regards,
Marko Antesic