Other Parts Discussed in Thread: THS4521
I am using ADS1278 with the following setup: f_clk = 4.096MHz, VREFP = 2.5V, Mode = Low-speed -> data output rate = 8kHz
I do observe toggling between two levels, delta V approx. 20µV
Toggling period decreases with increasing temperature. Time between toggles can be several hours.
This is what it looks like:
The figure is recorded during a temperature ramp from +85degC down to +25degC. Each data-point in the figure represents the average of 15 seconds of data (120,000 samples)
The phenomenon has also been observed at steady-state temperature.
The phenomenon has also been seen on different ADC input configurations.
Have anyone seen such a phenomenon, could it be a Delta-Sigma issue?