Tool/software: Code Composer Studio
When using CCS 7.0.0.00042 to check the compiler options for a MSP430F4793 project using the MSP430 TI v16.9.0.LTS compiler noticed an "odd" display for "Functions Subsections" in the project properties under Build -> MSP430 Compiler -> Advanced Options -> Runtime Model Options :
This is odd since there is no compiler option in brackets after the description, and the combo box for the "Function Subsections" entry contains no options.
There is a note on the http://processors.wiki.ti.com/index.php/Compiler_option_cleanup Wiki page that the --gen_func_subsections option is not available for the MSP430 compiler, so guess "Function Subsections" shouldn't be shown on the project properties for a project using the TI MSP430 compiler.