Other Parts Discussed in Thread: ENERGIA, , EK-TM4C129EXL, TM4C129ENCPDT
Tool/software: Code Composer Studio
- Ubuntu 16.04 LTS, 64-bit
- CCSv7.1.0.00016
- TM4C1294NCPDTI3 with Stellaris ICDI
- A detailed and reproducible test case: Fresh install of CCSv7 Offline Installer. Fresh install of Energia 18. Open CCSv7, Create a new workspace, select 'Project > New Energia Sketch', Energia Version set to 18, select 'Built-in Examples > 01.Basics > Blink.ino', selected device: 'LaunchPad (Tiva C) w/ tm4c129 (120MHz), select 'Finish'. Right Click 'Blink" project in the Project Explorer, select "Build Project'. Project builds fine. Push F11 (or select 'Debug Blink' from the toolbar). Code is uploaded, but there is no entry point, and the debug 'Resume' button is grayed out. 'Blink' runs fine in Energia itself. TI's compiler runs examples imported from Tivaware just fine. So, what's going on here, and how do I fix this?
I will post logs below.