Other Parts Discussed in Thread: HALCOGEN,
Tool/software: TI C/C++ Compiler
Hi there,
I'm using CCS 7.2.0 and CDT ARM 17.6.0.STS with TMS570LS3137-EP. Base code was generated from HALCoGen 04.06.01 & modified from there.
Each consecutive build of the exact same source files in the exact same environment produces a different .OUT file.
Using a "diff" tool, almost at the end of the file appear to be four or so instances of random hexadecimal strings of the form "{12345678-1234-1234-1234-123456789ABC}".
There are no date/time macros used, no post-build steps, I can only assume these are a 'Random' string (by the linker?) as part of the device's safety features (not yet matured in current design).
Even for development code, our corporate build processes requires the same output file to be generated from the same source across multiple machines, so it's something I need to understand shortly.
Could anybody please direct me to the relevant material to help understand further?
Many thanks, Mark