Other Parts Discussed in Thread: DLPDLCR2000EVM, , DLPC2607
Hello,
I successfully connected the BeagleBone Black to the DLPDLCR2000EVM and the DMD, and it is working perfectly well. I am trying to configure the DLPDLCR2000EVM /DMD (turn off the LED, export the display, and turn on the DMD) as soon as the BeagleBone Black is booted up. For that, I opened the crontab on BBB and added a command in the last line to run the EVM code on BBB’s boot. However, it runs any code when the BBB boots up, except the EVM commands.
Here is what I think is happening: usually, the BBB does all its configurations at boot, and then it makes the setups for the DLPDLCR2000EVM. However, when I command to run my code right after the BBB configuration, the EVM configuration wasn’t complete yet, so it will not work.
Please, does someone know how I could fix this issue or an alternative for running the EVM commands when BBB is boot up?
Thank you!
Thaisa