Good morning
Customer is claiming, that the delivered part is defective as follows:
Part is not working (not turning on) when connected to power supply
MeanWell GST90A19-P1M.
Connection has been done by following the datasheet information on page 8
here:
s%253A%252F%252Fwww.ti.com%252Ftool%252FDLPDLCR471TPEVM
Per customer, they have tested 2 power supplies and they are sure, that the issue is with the part itself. Power supplies are working when they
are used to power other devices.
Could you please advise if customer can perform some other test or if the part is fail?