Hi,
Can I know the dimensions of the DLPDLCR4710EVM-G2 module (Length x Width x Height). I want to use it in an application where there is dimension limit.
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Can I know the dimensions of the DLPDLCR4710EVM-G2 module (Length x Width x Height). I want to use it in an application where there is dimension limit.
Thank you.
Hello Vedashee,
Welcome to DLP forum and thank you for your interest in DLP technology.
Please refer to the following reference design for details of size and components layout of the EVM
https://www.ti.com/tool/TIDA-01226?keyMatch=DLP4710
If you just need the outer dimension to box the EVM? I will get back you in couple of days.
regards,
Vivek
Hi Vivek,
Actually I just need the outer dimension of EVM (L x W x H).
Hope to hear from you soon.
Thank you,
V. Vedashree.
Vedashree,
We will get back to you on this by early next week.
Regards,
Mayank
Hello Vedashree,
The dimensions are :
The projector has a projection barrel projecting out,
Main base - 155 mm (L ) x 100 mm (W) x 120 mm (H)
Projection Barrel - 60 mm ( L) and 50 mm diameter.
Square bounding box for complete EVM
215 mm (L) x 100mm (W) x 120 mm (H).
regards,
Vivek