Hello,
Upon startup the D2 LED is red and remains red unless I connect the board via usb to the Discovery 4100 GUI and wait for the D4100_GUI_FPGA.bin to programmed at which point D2 turns off and D16 turns green. As user "Fizix" mentioned in a previous post, I believe something has corrupted the PROM file or somehow the PROM is damaged. I was wondering if someone could recommend some steps I could take to determine which of these two situations is more likely and what I might do to move forward.
Thank You