Other Parts Discussed in Thread: DLPC900
Hello,
I've searched the forums for this answer but I've only seen answers from 3-6 yrs back.
Has there been a development of an API or SDK, for the DLPLCR9000EVM or DLPLCR6500EVM, since then?
Best,
Jimmy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Jimmy,
The API for the DLPC900 (controller) based systems is defined in the DLPC900 Programmer's Guide - DLPU018.
Let us know if this is what your were looking for.
Fizix
HI Fizix,
Thank you for the quick reply.
Would there be any sample code or a base API available, that can be modified?
Just so I wouldn't have to start from scratch.
Best,
Jimmy
Jimmy,
The entire source code for the GUI is available here:
There is a directory under the GUI directory names "Source". The default installation is at: C:\Texas Instruments-DLP\DLPC900REF-SW-5.0.0\DLPC900REF-GUI\Source
Fizix