Other Parts Discussed in Thread: DLP3030-Q1
Dears,
I have some questions about DLPC120 Automotive Control Program
We used the DLPC120 ACP to setup the DLP3030-Q1 EVM
1. The user guide mentioned using CA210 (Light meter) to debug the light source.
Is it possible to choose another Light meter(such as CL200, CL500, T10) and how to connect the settings?
2. The content of the calibration in the user guide is to calibrate the EVM system?
3. If we want to correct the LED parameters of different machines, how to write and update FLASH? (such as update Project or ...)
Many thanks & Best Wishes
Weite
E:weite.chi@ofilm.com