Other Parts Discussed in Thread: DLPC3432, DLPA3000
I got an inquiry for the power consumption of DLP230GP system.
Do you have estimation or measured data?
They got 4.8A/5V from optical module vender.
This LED current should be major of power, I think.
They calculated as follow (efficiency: 85%)
(4.8/0.85)*5
And other for DLPC, DLPA should be some additional.
I think basic idea should be correct.