Dear,
I see the operation temperature of DLPA3005 is 0 ~70 ℃,however, I want to know whether the chip can operate in -10℃(Minus 10 degrees Celsius),in this condition, what happened will be ?
could it work normally ? or any other issue ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear,
I see the operation temperature of DLPA3005 is 0 ~70 ℃,however, I want to know whether the chip can operate in -10℃(Minus 10 degrees Celsius),in this condition, what happened will be ?
could it work normally ? or any other issue ?
Hello Cooper,
Welcome to TI E2E Forums and thanks for showing interest in DLP Technology. Let me discuss your query internally and I will get back to you soon.
Regards,
Mayank
Hello Cooper,
The device is not qualified for the -10 and typically you will see device failure when operated outside specification.
regards,
Vivek
Hi Vivek:
how it can guarantee the temperature above 0℃,even in room, it may be below 0℃.
DLPA3005 ,is there the part industry level or can meet -10℃ ?
Hello Cooper,
We don't have a alternate part which qualified for lower operating temperature. You may have consider using a thermal heating pad for the device in your system design.
regards,
Vivek