Other Parts Discussed in Thread: DLPC350, , DLP-ALC-LIGHTCRAFTER-SDK
Hi Community
I saw that for DLPLCR4500EVM (therefore controller DLPC350) could load 48 patterns in the two buffers. But I suppose this is internal to the DLPC350, right? So for the 32MB on board memory I should be able to store more 1-bit patterns? Say if at one point I need to load new patterns from the flash into DLPC350, how fast could that be?
Another thing: the programming SDK for DLPC350 is also DLP-ALC-LIGHTCRAFTER-SDK (DLP-ALC-LIGHTCRAFTER-SDK Software development kit (SDK) | TI.com)? I just saw active support for the DLPC350 has stopped, but I suppose it is still compatible? Also I'm wondering if there's a manual for the SDK? The user guide online is only an installation guide...
Thanks,
Yujie