Hello,
I have encountered some problems when using LightCrafter4500 with GUI ver4.4.1.
In the Pattern Sequence mode with internal trigger, when the number of patterns are more than six and Repeats , incorrect patterns are displayed.
I set the Exposure time =Pattern Period =10 ms.
The sequence are read from the Flash memory and the version of the Firmware is 4.4.0.
Could you tell me how to deal with?
Best Regards,
Kokoro