This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPDLCR2000EVM: DLP2000, DLPC2607, DLPA1000

Part Number: DLPDLCR2000EVM
Other Parts Discussed in Thread: TIDA-00325

Hello everyone.

I'm interested in the DLPDLCR2000EVM board to make it a second monitor for a laptop.

At first, I thought I'd use a screenshare software to share my screen on a Raspberry Pi but it doesn't really meet my need since I will have two of the same screen. What I need is the pico-projector as a second monitor.

In order to do this, I would like to use it without a Raspberry Pi or a BeagleBone. My goal is to create a custom board with an IT6801FN chip (or equivalent) which will convert from RGB888 format to HDMI (something like the TIDA-00325). Do I need some other components to make it works or will the IT6801FN be enough by itself as a converter to use the evaluation board as a second monitor via HDMI ?

I don't have the evaluation module yet, I first try to know if it seems doable or not.

Since english is not my first language, let me know if you want me to rephrase it or if I need to give further information.

Best regards, 

Romain.