Hi,
We are running the DLP for image captures. Do we need to set the DLP pattern for every image capture? Is there a way we can just load the pattern once and capture multiple images. It seems the pattern loading is pretty slow (10s ms), so we think it's loading from flash through I2C every time. Is the DLP put in reset mode or standby mode after an image capture? If we put it in standby mode can we avoid loading the pattern again for the next capture? How to do it? Thanks