Other Parts Discussed in Thread: DLP471TE, DLPC7540
Dear TI support team,
I hope you are all doing great, as I need your assistance.
We have had a TI DLP471TE EVM with a DLPC7540 board for some time and they worked without any issues until recently.
Since two days ago the DMD has not displayed anything or even shown the start screen. I have tried to troubleshoot the issue and have undertaken the following steps thus far:
1. Exchanged all cables in different configurations to test if the cables work (different USB cable, different HDMI cable, also since I have 3 jumpers I interchanged them)
2. Checked the power supply (it works fine and delivers the required amps and voltage)
3. Tried running not only on external display mode but also a pattern or an image
4. Reinstalled the firmware (following procedure according to the manual - moving the boot jumper and back again after restart)
5. Measured the test points on the DMD board (3.3V and DMD VDD) - both work
6. Checked the pins on the DMD itself - they are fine
The lights on the controller board that are on: D5, D7, D25 - constant green colour; D15 - blinking green; D6 - constant red colour. Furthermore, all the boards (DMD, Controller, HDMI) seem fine and have no signs of burned electronic components.
I have attached pictures of the Error being marked as checked in the GUI and the advanced GUI (no other checkmarks appear):
The DMD has been operational (until now) under broad wavelength illumination and in accordance with the specifications.
Could you please help me figure this out and fix the issue?
I am looking forward to your reply!
Thanks in advance!