This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC3478: Pattern file generation without GUI, compatible with DLPC firmware 9.0.1

Part Number: DLPC3478
Other Parts Discussed in Thread: DLPC-API

We are programatically generating pattern binary files with the DLPC-API, this works with the previous firmware 8.1.0, but there is no updated API for the new firmware 9.0.1. Looking at the binary files from the GUI generated files, something has changed. Can we please get the source code, specifically "dlpc347x_internal_patterns.c" used in DLPC GUI V3.2.0.6. or instructions on what has changed?