Other Parts Discussed in Thread: DLP6500FLQ, DLPLCR65FLQEVM, DLPLCRC910EVM, DLPLCR65EVM, DLPLCRC900EVM, DLPC900, DLPC910
Hi,
I want to buy the EVM systems about DLP6500 series for laser patterning, aiming for a high power output upto approximately 1W/cm2 at 532nm.
I've narrowed down my choices to two EVM models based on DLP6500FLQ and DLP6500FYE.
Here are the respective order lists which i choose for each model:
For DLP6500FLQ :
1) DLPLCR65FLQEVM
2) DLPLCRC910EVM
3) power supply
For DLP6500FYE :
1) DLPLCR65EVM
2) DLPLCRC900EVM
3) power supply
Before finalizing my selection among these products, i have a few questions :
1. What are the key differences between the two EVM systems?
I've found differences in min illumination wavelength and pattern rate.
2. Are these systems suitable for my purpose to utilize the DMD?
If they are acceptable, please let me know the links to order the powr suuplys.
3. Is it the correct order list to use the DMD EVM system? If there are additional components needed, please advise.
4. From the DLP6500FLQ, can I remove the DMD mounts?
Thanks,
Heeju Son