Other Parts Discussed in Thread: DLPC3437, DLPC3439
Tool/software:
When I look at the driving data of DMD, no matter DLP330, DLP470 or DLP5530, their driving mode is basically the same. The SubLVDS signal of DMD lens drive is divided into two groups, which are output by the drive control IC DLPC3437, DLPC3439, DLPC230, etc. I have a doubt. Will the two sets of LVDS signals be output in parallel or will one set of LVDS signals be output first (corresponding to half of the DMD) and then another set? When I look at the driving data of DMD, no matter DLP330, DLP470 or DLP5530, their driving mode is basically the same. The SubLVDS signal of DMD lens drive is divided into two groups, which are output by the drive control IC DLPC3437, DLPC3439, DLPC230, etc. I have a doubt. Will the two sets of LVDS signals be output in parallel or will one set of LVDS signals be output first (corresponding to half of the DMD) and then another set?
I seek answers for these questions in China E2E support forum,but there is no reply for two days.
Here, Please help me answer this question,thank you !