Other Parts Discussed in Thread: UNIFLASH, DLPC3421, LP-XDS110
Tool/software:
Hello,
I obtained demo code for the DLPDLCR160CPEVM board through the TI secure site. This included source code for the out-of-box firmware, revision E15. Also included was a precompiled .out file in the "Debug" subfolder.
I tried to flash the EVM with this Rev E15 .out file. I used a J-link instead of the XDS110 (J-link is also supported by Uniflash). Through Uniflash, the J-link was able to connect and started the upload. Unfortunately, the flashing process failed almost immediately and the board is no longer responsive.
The green LEDs D1 and D2 are continuously lit after the board is powered via the USB-C connector. There is no reaction to activating the switches, and the projector does not turn on. Also, the J-link is now unable to connect to the board as target in order to erase or reprogram.
Is there any reason why the firmware flash would have failed, and is there anything that can be done to recover the board?