Other Parts Discussed in Thread: DLPA3005, DLP4710EVM-LC
Tool/software:
When I set 00h to 5Bh using the DLPC3479's "Write RGB LED Current PWM (54h)" command and read it back, the set value becomes 5Bh.
Why is that?
The DLPA3005 manual says, "For proper operation, the LED current must be at least 5% of ILED_MAX." So is it not possible to set a value lower than 5Bh, or 00h?