This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problems in self-designed DLP board

Other Parts Discussed in Thread: DLPC200

Hi

i have already programmed the DLPC200 firmware down into DLPR- M25P64 using the 8M BIN file

the CFG_DONE led light up correctly , and i get into the controlling software with all green rightmarks ~

but when i run a project , the RUN LOG shows many errors..... :( 

can you give me some advice?

thank you ~~

  • Hi Diao,

    The Green marks appear only after the GUI communicates with DLPC200 to read the status. So it means to begin with the GUI is able to communicate with the DLPC200 device and then something went wrong.

    Please do the following:

    Power on the system, if you have stored default solution verify whether the solution is displayed if not verify Checker board pattern appearing. Then read the status attach this snapshot in your response.

    Try DMD park and un-park operation in GUI verify it works.

    Please send us the project.

    Regards,

    Sanjeev

     

  • Hi Sanjeev,

    thank you for the advice .

    i'll try it .

    can you give me your e-mail address so i can send the project to you

     

    Regards,

    Diao