This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello everyone,
I want pattern sequences of following.
> 69 x 1bpp RGB MBMC Pattern Sequence with Exposure = 10000us
> 69 x 1bpp RGB MBMC Pattern Sequence with Exposure = 10500us
Regards,
user4788358
If I understand correctly, you'd like just one trigger after each set of R, G, B. Unfortunately, the way the Lightcrafter EVM was designed, this is not possible. If you had an alternate LED driver design this might work, but it's one of the limitations of this EVM.
-Paul
This type of triggering configuration is only possible with video data being streamed into the device. For a pre-stored pattern mode, you'll get a trigger after every 1-bit plane. Section 4.2 of the user's guide shows an image like you've posted.
Hope that helps,
Paul