Hello,
Can i make 3d printer with DLP9000X !?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Hamid,
If 4k is a requirement, then no DMDs will currently work. For highest resolution available (2560 x 1600) then the DLP9000 or DLP9000X are going to be the only options. However, typically with SLA printing UV light is used, which these devices do not support very well. If you are using UV to cure the resin, you'll need to use a UV part such at the DLP9500UV or DLP7000UV.
Resolution and build envelope are largely going to depend partially on optics and the speed of any device should be more than sufficient for SLA.
Take a look at this page for some more information regarding 3D printing: www.ti.com/.../applications-featured-applications.page
-Paul
Dear Hamid,
I am Philipp from ViALUX company in Germany. We are an official design house partner of TI.
We provide a complete DLP Module with Mainboard, Software and DMD chip for DLP9000X called V-9001 Module.
It is suitable to do 3D printing applications (depending on your wavelength). 405nm is suitable.
Please contact us directly for details at dlp@vialux.de
Kind regards
Philipp, ViALUX GmbH