Other Parts Discussed in Thread: DLPC4422,
Hello.
1. I am looking to see if there is a way I can use the DLP650NE without using the DLPC4422 controller?
2. Also, in order to operate the DLP650NE, I see that the DCLK is 400 MHz and there are two other control signals associated with it is SCTRL_AP and SCTRL_AN. Are these 2 control signals SCTRL_AP and SCTRL_AN are required to drive the 64 bit LVDS input to the DLP650NE?
3. What is the state of these 2 control signal SCTRL_AP and SCTRL_AN?
Thanks,