Other Parts Discussed in Thread: DLP5500, , DLPLCR70EVM, DLPC410, DLPC900
Hello,
My application is a schlieren measuring system ("Toeplers Dual Field Lens System") to visualize ultra sound waves. For this application I want to use a DMD as a spatial light modulator. I want to put my DMD in the focalplane of my second lens and want to use as a blend, like knife edge cutt-off. So a simple application.
The application with lenses, laser, ccd-Camera is already implemented.
The Data of my pulsed Laser: Wavelength 532nm , pulse length 1,2ns, 4,5 uJ Pulsenergy
CCD Camera has the resolution:1928x1448
I am thinking of to use the DLP 7000 for my application. Because of the pitchlength which is 13,68 um. I read, that if the pitch length is higher, then there is less diffraction.
Would you recommend me the same DLP, or a another one like DLP6500 or DLP5500 or something different?
My next question is also, for this application is a DLP7000 chipset enough? What should I also have to order? How can I program via PC the DMD?
I think for my application is a EVM Board to much, or what do you recommend ? Because the usage is only for a blend.
Another question is, after programming the DMD, can I switch it off and the mirrors will stand on the same place? Or it will go to the flat mode back?
Thank you for you support