Other Parts Discussed in Thread: DLPA3000, DLPC3439
Hello,
My application is trying to use the DLP pico chipsets, in a low power system. I'm trying to figure out which chipset would give us the best resolution within our power limits. We are looking to keep total power usage around 5W.
I see the DLP4710 chipset EVM has a upper limit of 19 V DC, 4.74 A, but could you give me a low power estimate for a system using this chipset? I see the DLPA3000 has a minimum I-led of 300mA at 8V, does this mean all three led's will be using 300mA at the same time or would each led use 300mA sequentially and switch off when the other leds are on?
If this chipset exceeds our power limit, what chipset would you recommend next?
Thanks.