Part Number: DLP3000-C300REF
Dear TI,
I've got one DLP3000 (out of six DLPs on a rig), which gets stuck in the booting sequence.
When I boot from NAND, the DLP stuck at 98% during booting.
When I boot from SD card, sometimes it succeeded, sometimes all the LEDs on the control board (top PCB) are OFF at 98%.
Does that mean the NAND is broken? How can I test/fix it?
Or is there a way to reliably boot from the SD card?
Thanks.
Best,
Joseph Huang