Other Parts Discussed in Thread: DLPC3439
Dear All,
We developed our own projector (full custom) from the control board to the optical engine (PCBs and optics). After minor fixes due to some forgotten connections we managed to start the projector and use it just like the DLPDLCR4710EVM-G2.
Here some photos of the design :
Now before mass producing the projector we have to add some new features to the hardware (such as replacing the USB interface with RS485). Everything is fine so far but we need some clarification to some points.
1- In our optical engine we are using different OSRAM LEDs (5 A each ! expl : BLUE). In the future we gonna use 16A LEDs but for now we need to set the max current of the LEDs to 2A during startup ? We are guessing that the DLPC3439 firmware is responsible for setting the default values of the LED current. Is there anyway to limit the current (except replacing the Rlim resistor with higher value) ?
2- Is there any tool to modify the DLPC3439 firmware ? (redefine the default values and images ...)
Kind regards