Hi Team,
My Customer would like to use DLP7000 (or similar) part with UV fused silica window to work with 245-250nm light. Is a custom order possible?
Thanks in advance.
Regards,
-Renan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
My Customer would like to use DLP7000 (or similar) part with UV fused silica window to work with 245-250nm light. Is a custom order possible?
Thanks in advance.
Regards,
-Renan
Hi Fizix,
Thank you for this reply. I already forwarded this message to my customer, and their response is (1) can you provide why we don't support a custom device? Like replacement of the window? (2) Is it possible to sell them the device without the window?
Regards,
-Renan
Renan
DLP DMDs are fabricated in our high volume semiconductor process. It would be incredibly expensive to build custom variations. As Fizix asked above if you can provide more details as to the application and possible volumes we could look at building a DMD that supports 245 - 250 nm operation.
Regarding a DMD without an optical window, for reliability of the DMD MEMs structures they need to be isolated from external contaminates.