Other Parts Discussed in Thread: DLP650LNIR, DLP9500, DLP7000, DLPC410
Hello,
In dlpu039a (DLP Discovery 4100 Controller Board API Programmer’s Guide (Rev. A)) under section 6.2.2 the "LoadData" function is described. I have a couple of questions regarding the description of the function.
1. "Data must be in a UCHAR array of size length." What does each UCHAR's value map to in terms of controlling what state the mirror lands to? I know 0xff will land it in the on-state, while 0x00 will load it in the off-state, but loading some value in between seems to give some odd patterns. Is there some documentation that I missed about how this value is converted to command the mirror to land in either the on or off states?
2. "No more than 500 rows can be loaded at a time (96 kb for DLP9500, 51.2 kb for DLP7000, and 64 kb for DLP650LNIR). To load an entire DMD call this function multiple times" If loading a full image to the DMD (say the 0.7 XGA DLP7000 - 768 rows), is there any difference in loading 500 rows, and then the other 268 rows with the second call, or just loading 384 rows and then loading the other 384 rows?
Thanks,
-Danyal