Hello,
I have developed a projector board using DLPC3478.
It operates in external pattern streaming mode that transfers data from FPGA to DLPC3478.
As shown in the figure, when one frame is transferred and then the next frame is transferred after a while (approximately 10 to 15 seconds), the previous frame is projected from DLPC3478.
At this time, granular noise is superimposed on the entire projection data.
The longer the interval, the greater the amount of noise.
Please tell me the reason.
Has the DLPC internal memory been refreshed correctly?
Also, if this behavior is a chip specification, what is the allowable interval time?
Regards, Masa