Other Parts Discussed in Thread: DLPC410, DLP7000
In the description of the spec sheet of dlp9500, the "pattern rates (1-bit binary) was described as 23,148 Hz and "GLOBAL RESET MODE (Patterns/s)" was 17857.
The description of DLP Discovery 4100 also contained the following sentence: "The DLP Discovery 4100 Development Platform is capable of operating at about 7-10 DMD frames per second (DMD dependent) when connected to a host system's USB 2.0 port."
My questions are below.
1) What is the difference between "23,148", "17857", and "7-10"?
2) When I try to use a PC connected with the controller by USB 2.0 port, it's only 7-10 frames per second due to the speed limit of USB 2.0. Am I right? Then, how do I achieve higher frames per second? (When I use a PC.)
3) When using the DLP9500 in real situations, what should I do to achieve 17857 patterns/s (or near that)? Which things are needed? How do I configure the system? Is it possible?
(I just need the binary pattern rates. NOT color pattern or grayscale.)