Other Parts Discussed in Thread: DLPC3430, DLPC3433, DLPA2000, DLPC3438, DLP230GP, DLPC3432
Hi Expert,
I'd like to drive DLP3010 with 120Hz 3D input source.
The 120Hz timing is confirmed by the vendor of the optical engine.
It's at Look 1.
Then, I modified the EDID setting for 120Hz timing and also enable Vsync to check if it's 120Hz or not.
Then, I got that Vsync is 120Hz. But, the display is abnormal.
Here are 2 questions.
1. What is DSI host timing requriements for 120Hz 3D mode?
So far, I only have the requirement for 60Hz.
2. Is there anything else I need to modify?
BR,
Wilbur.