Hi all,
during the last year I equipped several of our mounting machines with NIRscanNanos to ensure that the correct plastics are being processed. Each machine is equipped with two sensors. This worked fine for the first times. The first machine, which had been upgraded, works without problems since march 2020. But when I equipped the last machines, two sensors first worked fine and then suddenly were dead after two weeks. When I power on the sensors, they don't do anything any more. No control LED, no reaction. The sensors were mounted in two different machines.
To protect them from environmental influences, I had put the sensors into shielded metal boxes with ventilation slots. Moreover I had protected the sensors from electrostatic discharges and electromagnetic interferences by using Würth Elektronik USB 2.0 EMC Stick with integrated ESD Protection and EMI Filter.
I simply can't imagine why the two sensors don't work any more, while the other 10 sensors work fine. How shall we proceed with the two sensors which don't work?
Kind regards,
Simon