Other Parts Discussed in Thread: DLPC350
Dear all,
I am testing with DLP4500EVM and I encounter cannot continuously display 2 pattern sequence patterns in single 24bit video stream data in the pattern sequence mode.
Below is the pattern sequence settings I set in the DLP4500 Light crafter GUI.
I am continuously transfer video data to the DLP4500EVM with Vsync signal frame rate around 59.81Hz and the pixel clock is 73MHz. Below is the DLP4500EVM feedback signal.
Blue signal is Vsync signal. Pink signal is DLP4500EVM TRIG_out_1 signal. I am getting delay of 1 frame DMD video output everytime.
In the user guide manual, it suppose to have 1 frame delay of DMD video output for the first frame of video input only that show in the diagram below.
Is my pattern sequence settings got problem?
Thank you.
Best regards,
Pang