Other Parts Discussed in Thread: DLPC350
I'm using LighCrafter 4500 EVM and using flash memory as input source for pattern display. I measured image loadiing time using GUI, and found out one of the images loading time varied from around 350ms to 440ms, while for others it only took around 100ms. And the display of patterns screwed up because of this super long loading time.
Although I can correct this by reorganizing the patterns in each image, I would like to know is that normal to take around 400ms to load one buffer? Because in the user's guide chapter4, it reads as at-worst-case 200ms to load one buffer, and I organized my patterns according to this number.
I'm using the newest GUI and DLPR350PROM-2.0 to build the new firmware.
Thank you for your time!