This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
i have the same problem as the following, how can we preoceed to fix?
Thank you
Giorgio - i need to do some research but can you verify the credentials you are using, usually you need your test secret and test key id along with your authentication access key 3 pieces to mak a test call and then for a production call you would also need those 3 pieces related to production, i will look into this and respond later today.
Giorgio,
I am running this prod store API - Get product with your prod credentials.
for the part you reference above (DS90UB935-Q1) its orderable material is below
So I ran a test below with the material needs to exist on www.ti.com and verify the version you are using is v2 vs v1.
see example below.- hope this helps
https://transact.ti.com/v2/store/products/DS90UB935TRHBRQ1 (as an example with your client id and secret)
"tiPartNumber": "DS90UB935TRHBRQ1",
"genericPartNumber": "DS90UB935-Q1",
"buyNowUrl": "">www.ti.com/.../DS90UB935TRHBRQ1",
"quantity": 0,
"pricing": [
{
"currency": "USD",
"priceBreaks": [
{
"priceBreakQuantity": 1,
"price": 5.391
},
{
"priceBreakQuantity": 100,
"price": 4.395
},
{
"priceBreakQuantity": 250,
"price": 3.454
},
{
"priceBreakQuantity": 1000,
"price": 2.93
}
]
}
],
"futureInventory": [],
"description": "FPD-Link III 3-Gbps serializer with CSI-2 interface for 1 MP & 60 fps",
"minimumOrderQuantity": 1,
"standardPackQuantity": 3000,
"exportControlClassificationNumber": "EAR99",
"htsCode": "8542390001",
"pinCount": 32,
"packageType": "DS90UB935TRHBQ1_32_VQFN_RHB",
"packageCarrier": "CUT TAPE",
"customReel": true,
"lifeCycle": "ACTIVE"
}
**Attention** This is a public forum