Part Number: TUSB4041I-Q1
Hi,
I am using TUSB4041 as USB hub in my design. I need total 6 USB ports, so two USB hubs are used. USB upstream is connected to a processor and down streams are connected to 5 devices and a connector. My problem is USB hubs detected in some boards but in others it is not detecting. I have checked the 24MHz clock, 3.3V and 1.1V power rails, all are good. And also checked the power on sequence, 1.1V will come before 3.3V. I have checked with PC also by isolating the processor and directly connected to the PC, but not detecting. Can anyone suggest some solutions ? I have attached the schematics here.