Part Number: DP83867IS
When using 100 Base-TX mode only, a previous thread stated that pins 1/2/4/5 can be used. Which two pins are the TX and which two pins are the RX? Thanks in advance.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83867IS
When using 100 Base-TX mode only, a previous thread stated that pins 1/2/4/5 can be used. Which two pins are the TX and which two pins are the RX? Thanks in advance.
Hi Kevin,
Like stated in the datasheet, the pins can function for TX signals and RX signals.
Thanks,
Lysny
Hi Kevin,
For 100M pair A functions as transmit and pair B functions as receive as a default. But if using auto-mdix, each pair can function as either RX or TX.
Thanks,
Lysny