Part Number: DS90UB947-Q1
Other Parts Discussed in Thread: ALP
Hi team
can 947 pattern support this resolution 2396*1094*60fps with internal clock? the PCK is about 160MHz.
Check document of 947, it support 800MHz OSC, how to select M/N to generate this resolution?
customer try to use M=2 N=10, it can't work.
in additional, use ALP tool, can't select M/N and the max PCLK is 100MHz. we did not connect the 947, does it needed for M/N adjust?
thank you