Part Number: TPS65988
Other Parts Discussed in Thread: TPS65987D, , TPS65987
I have a TPS65987D EVM which I configured as UFP, with role swap to allow charging at the same time. This works well for me. Please see attached project file.TPS65987EVM.pjt
However, this part is hard to obtain right now so I switched to a TPS65988DH intending to use it in 87 emulation mode. I made a new project file, duplicating the settings from my TPS65987 project where possible. I turned on 87 emulation mode. I also have the jumpers arranged as per the TPS65988 EVM user guide. (See attached photo).

I am also attaching my TPS65988DH project file. Essentially, when I plug in a phone to Port A, I see no voltage on VBUS (P5V test point measures 5.0V), it doesn't seem a negotiation occurs and the device does not charge. What am I missing / what did I configure incorrectly? Thank you!